Material Usage report
The Material Usage report displays all of the batches that used a specified material during a specified time period. This report has a Material Usage table plus a header section. The header displays the specifics of the material and the amount consumed. The Material Usage table displays a list of batches that used the material. The report lists:
- Unique ID
- Batch ID
- Amount Consumed
- Lot ID
- Event Time
- Area
Expand the Batch to view associated Units used with the amount of material consumed.
Hyperlinks
This report has hyperlinks to these reports:
Icon | Destination Report |
|---|---|
White Tag | Batch Listing |
Yellow Tag | Batch Summary |
Filters
This report features filters for
Date
and Time
ranges, Process Cell
, Unit Name
, Recipe Name
, and Material Name
. The Batch ID
filter can filter data by inputting search criteria in the form of a Batch Name
. Use the asterisk (*) as a wildcard character.The
Number of Rows
filter allows users a way to be able to limit how many rows of data the database query returns to the report. This filter is set to 1000 by default. While this can be useful in limiting the amount of data returned from a dataset and displayed in a report, it can lead to confusion when used in conjunction with other filters such as Recipe Name, Process Cell, Unit Name, etc.
If a user wants to filter data shown in a report using any of the filters other than
Number of Rows
, the Number of Rows
filter should be changed from 1000 to 0. This ensures all rows of data are filtered as specified and displayed correctly.Users can select all areas or a specific Batch server area name by using the
Area Name
filter.Provide Feedback