Batch Summary report
The Batch Summary report includes two tables and a header section, the Phase, and Amount
vs. Actual tables. The header displays the specifics of the batch, such as:
Header name | For FactoryTalk Batch, displays | For SequenceManager, displays |
|---|---|---|
Batch ID | Batch ID | Sequence ID |
Unique ID | FactoryTalk Batch Unique ID | SequenceManager Unique ID |
Recipe Name | Recipe Name | Sequence Name |
Area Name | Area | Controller Serial Number |
Process Cell | Process Cell | Controller Serial Number |
Product Code | Product Code | Blank for SequenceManager |
Product Description | Procedure Description | Extended Text |
Formulation Name | Recipe Formulation Name. If formulation parameters are not passed, or are an
empty string, "Default Formulation" displays. | Blank for SequenceManager |
Formulation Description | Recipe Formulation Description. If formulation parameters are not passed, or
are an empty string, the description is empty. | Blank for SequenceManager |
Completion State | — | — |
Start Time | — | — |
End Time | — | — |
Duration | — | — |
FactoryTalk Batch
and SequenceManager
events. The Amount vs. Actual table displays the Recipe Name along with the Recipe
amount, the Actual amount used, and the Deviation from the recipe amount. If a measurement
can be fractional, the decimal places round to three places.Expand the Units in the Phase table to view the phases. Expand each phase to see the phase details.
Version
The version of the FactoryTalk Batch report provides the following information:
- When the report was last modified.
- The version of the report that is currently installed.
- If a custom report is based on a particular version of a report, it shows which version of the report was used.
Hyperlinks
This report has hyperlinks to these reports:
Icon | Destination Report |
|---|---|
White Tag | Batch Listing |
Magnifying Glass | Batch Detail |
White Arrow | Backward Tracing |
Clock | Batch Execution |
Filters
This report features filters for the following:
Filter name | Description |
|---|---|
Start Time | Filters based on start time. Select NULL to filter from the beginning of collected time. |
End Time | Filters based on end time. Select NULL to filter to the end of collected time. |
Batch ID Filter | Accepts search criteria in the form of a Batch Name . Use the asterisk (*) as a wildcard character. |
Process Cell | Filters based on the process cell name or controller serial number. |
Recipe Name | Filters based on the recipe name or the sequence name. |
Unit Name | Filters based on the unit name or the sequence unit ID. |
Unique ID | Specifies which records display in the report. |
Area Name | Users can select all areas or a specific Batch server area name. |
Show All Levels
option expands all items in the Phase table such as
operations and phases in the generated report.Provide Feedback