Batch Exceptions report

The Batch Exceptions report displays Abnormal Exceptions that occurred during a batch. The abnormal exception states are STOPPED, ABORTED, HELD, and FAULTED. Other states are not included in this report.
This report includes a header section that displays the specifics of the batch, such as:
Batch specifics in the header
Header name
For
FactoryTalk Batch
, displays
For
SequenceManager
, displays
Start Time
End Time
Batch Failures
Failure message.
The ordinal value of the failure message.
Area
The Batch Exceptions report includes Operation Sequences from both
FactoryTalk Batch
and
SequenceManager
events, and lists:
  • Abnormal State Changes
  • Alarms and Events
  • Batch Failures
  • Out of Tolerance events
Out of Tolerance events
Version
The version of the FactoryTalk Batch report provides the following information:
  • When the report was last modified.
  • The version of the report that is currently installed.
  • If a custom report is based on a particular version of a report, it shows which version of the report was used.
Hyperlinks
There is a hyperlink to return to the Batch Listing report. This hyperlink does not pass any parameters back to the Batch Listing report.
Filters
This report features filters for the following:
Filters
Filter name
Description
Start Time
Filters based on start time. Select NULL to filter from the beginning of collected time.
End Time
Filters based on end time. Select NULL to filter to the end of collected time.
Batch ID Filter
Accepts search criteria in the form of a
Batch Name
. Use the asterisk (*) as a wildcard character.
Process Cell
Filters based on the process cell name.
Recipe Name
Filters based on the recipe name.
Unit Name
Filters based on the unit name.
Unique ID
Specifies which records display in the report.
Area Name
Users can select all areas or a specific Batch server area name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal