Batch Detail report

The Batch Detail report displays the details of a specified batch. This report includes a header section, phase table, alarms and events, and state changes. The header displays the specifics of the batch, such as:
Batch specifics in the header
Header name
For
FactoryTalk Batch
, displays
For
SequenceManager
, displays
Batch ID
Batch ID
Sequence ID
Unique ID
FactoryTalk Batch
Unique ID
SequenceManager
Unique ID
Recipe Name
Recipe Name
Sequence Name
Area Name
Area
Controller Serial Number
Process Cell
Process Cell
Controller Serial Number
Product Code
Product Code
Blank for
SequenceManager
Product Description
Procedure Description
Extended Text
Formulation Name
Recipe Formulation Name. If formulation parameters are not passed, or are an empty string, "Default Formulation" displays.
Blank for
SequenceManager
Formulation Description
Recipe Formulation Description. If formulation parameters are not passed, or are an empty string, the description is empty.
Blank for
SequenceManager
Completion State
Start Time
End Time
Duration
Batch Failures
Failure message
The ordinal value of the failure message
The Phase table displays a list of the units used during a specified time period for a particular batch, and includes Operation Sequences from both
FactoryTalk Batch
and
SequenceManager
events. The report lists:
  • Unit Name
  • Phase
  • Start and End times
  • Duration of each phase
  • Unique ID
Each level can be expanded down to the Equipment phase to view details, which include the recipe and report parameters and their corresponding values.
TIP:
Phases that do not have recipe or report parameters do not appear in the Batch Data table. To see a list of all phases (including those that do not have recipe or report parameters), use the Batch Summary report.
The Batch Detail report displays Abnormal Exceptions that occurred during a batch. The abnormal exception states are STOPPED, ABORTED, HELD, and FAULTED. It does not display any other states. The report also displays Alarms & Events, Batch Failures, and a Setpoint vs. Actual Summary section.
Version
The version of the FactoryTalk Batch report provides the following information:
  • When the report was last modified.
  • The version of the report that is currently installed.
  • If a custom report is based on a particular version of a report, it shows which version of the report was used.
Hyperlinks
This report has hyperlinks to these reports:
Hyperlinks to reports
Icon
Destination Report
White Tag
Batch Listing
Yellow Tag
Batch Summary
White Arrow
Backward Tracing
Clock
Batch Execution
Filters
This report features filters for the following:
Filters
Filter name
Description
Start Time
Filters based on start time. Select NULL to filter from the beginning of collected time.
End Time
Filters based on end time. Select NULL to filter to the end of collected time.
Batch ID Filter
Accepts search criteria in the form of a
Batch Name
. Use the asterisk (*) as a wildcard character.
Process Cell
Filters based on the process cell name or controller serial number.
Recipe Name
Filters based on the recipe name or the sequence name.
Unit Name
Filters based on the unit name or the sequence unit ID.
Unique ID
Specifies which records display in the report.
Area Name
Users can select all areas or a specific Batch server area name.
A
Show All Levels
option expands all items in the Phase table such as operations and phases in the generated report.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal