Backward Tracing report

The Backward Tracing report displays the lot and equipment used for a particular batch. The report includes a header section and a Lot table. The header displays the specifics of the batch, such as:
Batch specifics in the header
Header name
For
FactoryTalk Batch
, displays
For
SequenceManager
, displays
Batch ID
Batch ID
Sequence ID
Unique ID
FactoryTalk Batch
Unique ID
SequenceManager
Unique ID
Recipe Name
Recipe Name
Sequence Name
Area Name
Area
Controller Serial Number
Process Cell
Process Cell
Controller Serial Number
Product Description
Procedure Description
Extended Text
Formulation Name
Recipe Formulation Name. If formulation parameters are not passed, or are an empty string, "Default Formulation" displays.
Blank for
SequenceManager
Formulation Description
Recipe Formulation Description. If formulation parameters are not passed, or are an empty string, the description is empty.
Blank for
SequenceManager
Completion State
Start Time
End Time
Duration
The Lot table displays the Lots used by a particular batch and the Equipment table displays the equipment used by the batch. The Lot table includes:
  • Lot ID
  • Material ID
  • Amount Consumed
  • Recipe Name
  • Event Time
Expand the lot to display the units used by the batch. The Equipment table displays the equipment used by the batch and when it was acquired and released.
Hyperlinks
This report has hyperlinks to these reports:
Hyperlinks to reports
Icon
Destination Report
White Tag
Batch Listing
Yellow Tag
Batch Summary
Magnifying Glass
Batch Detail
Clock
Batch Execution
Filters
This report includes filters for
Process Cell
,
Unit Name
,
Recipe Name
, and
Unique ID
. Use the
Batch ID
filter to enter search criteria in the form of a
Batch Name
. Use the asterisk (*) as a wildcard character.
Users can select all areas or a specific Batch server area name by using the
Area Name
filter.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal