Filter report

When you view reports, all lifecycle information in the FactoryTalk AssetCentre will show. Filter report to show those you want to see.
To filter report
  1. On
    Lifecycle Information
    , select
    Report
    .
  2. Hover over the column headings, and then select report filter.
  3. Select web archive filter2 or web archive filter3, and then configure the filter conditions as needed.
    TIP:
    You can filter multiple columns at a time. Use web archive filter3 to filter columns to shown on Report and use web archive filter2 to configure the filter conditions on each column.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal