Add Region
By default, Enterprise is added to the hierarchy list. The user can add a Region, Product, or Site under the Enterprise. Perform the following steps to add a Region:
- On the left navigation menu, drop-down theConfigurationmenu and clickAsset Setup.
- Click theEnterpriseorProductnode from the Hierarchy list.
- Click the [] icon and selectAdd Node.
- In theAdd Nodewindow, set these parameters:
- Select item type: Select the Region radio button in the left pane.
- Name: Provide the Region name.
- Description: Provide a description of the Region.
- Functional Location: Provide the location details.NOTE: Select theAuto Generate Functional Locationcheckbox to use the system-generated functional location.
- Configuration Status: By default, Configuration Status is in Draft, and the user can select the required status from the drop-down list.
- ClickAdd.Add Region Window"Region was added to hierarchy successfully" message is displayed.
- (Optional) In theInfotab, clickEditand perform the following actions:
- Geographical Location: Provide the Geographical Location details.
- Contact Details: Provide the Contact Details.
- Remarks: Provide the Remarks details.
- ClickSave.
Provide Feedback