Add Asset
The user can add assets directly under the Site or Area or Sub Area. Perform the following steps to add assets:
- On the left navigation menu, drop-down theConfigurationmenu and clickAsset Setup.
- Click theSite,Area, orSub Areafrom the Hierarchy list.
- Click the [] icon and selectAdd Node.
- In theAdd nodewindow, set these parameters:
- Select item type: Select the Asset radio button in the left pane.
- Name: Provide the Asset name.
- Description: Provide a description of the Asset.
- Functional Location: Provide the location details.NOTE: Select theAuto Generate Functional Locationcheckbox to use the system-generated functional location.
- Configuration Status: By default, Configuration Status is in Draft, and the user can select the required status from the drop-down list.
- Asset Class: Select the required Asset Class from the drop-down list.
- ClickAdd.Add Asset Window"Asset was added to hierarchy successfully" message is displayed.
- (Optional) In theInfotab, clickEditand perform the following actions:
- Geographical Location: Provide the Geographical Location details.
- Contact Details: Provide the Contact Details.
- Remarks: Provide the Remarks details.
- Make: Provide the Asset Make details.
- Commission Date: Select the Commission Date using the date picker.
- Lifecycle Status: Select the required Lifecycle Status from the drop-down list.
- Files Uploaded: ClickBrowseto upload the files related to the Asset.
- ClickSave.
To configure
KPI
and Sensors
tab, refer to Configuration tab .After the Asset is created successfully, the user can create Components, KPIs, Sensors, and so on. There are two ways to create them. The one way is to apply an existing Asset Model to that Asset and another way is the user create everything manually. The following sections cover both topics.
Provide Feedback