FactoryTalk Action Manager users

To sign in
FactoryTalk Action Manager
, use
FactoryTalk Security
users in
FactoryTalk® Administration Console
.
TIP:
Windows users are authorized in
FactoryTalk Administration Console
by default. Select
Sign in with current Windows user
to sign in
FactoryTalk Action Manager
use the current Windows user.
Follow these steps to create a
FactoryTalk Security
user in
FactoryTalk Administration Console
as needed:
  1. In the
    FactoryTalk Administration Console
    Explorer
    , expand
    System
    >
    Users and Groups
    .
  2. Right-click
    Users
    , and then select
    New
    >
    FactoryTalk User
    .
  3. In
    New FactoryTalk User
    , enter a username and a password, and then select
    OK
    .
Each user can be granted the following access permissions:
  • View Project
    View status, triggers, actions, and tasks.
  • Modify Project
    Configure triggers, actions, and tasks.
  • Run Test
    Run actions and actions in tasks to check how the actions are performed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal