Fault Code Lookup view parameters

The
Fault Code Lookup
view includes these parameters.
Parameters
Parameter
Description
Fault code
Specifies the fault code (while online). When a fault occurs with the Multifunctional Access Box, the fault code displays in the
Connection
view under
Connection Fault
.
Fault type
Displays information about the fault code.
This parameter is blank when there is no active fault.
Description
Displays additional information about the fault code.
This parameter is blank when there is no active fault.
Remedy
Displays information about the potential remedies for the fault code.
This parameter is blank when there is no active fault.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal