View a fault code for the Multifunctional Access Box
Use the
Fault Code Lookup
view to view a fault code for the Multifunctional Access Box.To view a system fault code for the Multifunctional Access Box
- On the tab for the device, selectConnection.
- In theConnectionview, underConnection Fault, read and record the fault code.
- On the tab for the device, selectFault Code Lookup.
- In theFault Code Lookupview, in theFault codebox, enter the fault code.
- SelectLookup.
- View information about the fault code.
- If the fault is currently valid (input bit DiagnosticActive = 1), information displays forDescriptionandRemedy.
- If the fault is no longer valid (input bit DiagnosticActive = 0), no information displays.
To view a device fault code for the Multifunctional Access Box
- InController Tags, underFault Code, read and record the fault code.
- Repeat steps 3 to 6 inTo view a system fault code for Multifunctional Access Boxto look up and view a device fault code.
Provide Feedback