Predictive Maintenance (PM) view
The Predictive Maintenance view displays predictive maintenance data for the Supplemental Power Tap.
Predictive maintenance data is blank when offline.
The options in this table describe the predictive maintenance parameters.
Parameter | Option |
|---|---|
View as | This is a display filter that displays predictive maintenance data according to the selected option:
|
Status | Values are:
|
Consumed life percentage | Displays the percentage of the total estimated life that has been consumed. |
Location | Identifies the location of the component within a product, device, or subsystem. |
Catalog number | Displays the device catalog number. |
Reset | Resets the predictive maintenance data.
WARNING:
This action cannot be undone and may affect all subsequent PM data.
|
Settings | Displays the predictive maintenance settings dialog box. |
Refresh | Manually refreshes the predictive maintenance data when online with the device. |
Provide Feedback