Predictive Maintenance (PM) settings

The Predictive Maintenance settings displays options to set indicators and messages, and configures the alarm for the remaining life threshold percentage.
IMPORTANT:
To change any settings
  1. Select the General tab.
  2. Make the changes.
  3. Select Ok.
Parameters
Parameter
Description
Predicted life
Displays the Maximum life and the Remaining life threshold.
Alarm notification
Enables the remaining life below the threshold alarm. If not selected, the alarm is not set even if the alarm threshold is crossed.
Remaining life threshold %
Sets the remaining life threshold as the percentage of Maximum life. Values allowed:
  • Custom percentage-when Custom percentage is selected, enter a value for the Remaining life threshold. Allowed values are from 0% to 100%, in 0.001% increments.
  • 5%
  • 10% (default)
  • 15%
  • 20%
  • 25%
  • 30%
  • 35%
  • 40%
  • 45%
  • 50%
NOTE: Remaining life varies according to selected threshold values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal