Online values view
The Online Values view displays the statuses or states for the power supply, warnings, and trips.
TIP:
Online values only appear when the unit is connected online.
Sections | Parameters | Values |
|---|---|---|
Power |
| |
Warnings |
| |
Trips |
|
NOTE:
Values are hidden when offline or the device type in project does not match physical device.
NOTE:
Some features will not show a value when the feature is not enabled in the configuration.
Provide Feedback