Device Definition

The device definition dialog box allows you to configure device parameters.
Parameters
Field
Description
Device type
Static field that displays the connected device type.
Name
A text field for a user-defined name.
Description
The selected device description is automatically entered.
IP address
This field configures the IP address. Select the final digits of the IP address from the dropdown list. Values are from 2 to 40.
Series
Select the letter designation for the device series from the drop-down list.
Revision
Select the major and minor revision from the drop-down lists.
Electronic keying
Configures the type of electronic keying used to compare the device in the project with physical device before I/O communication begin. Select the electronic keying type from the dropdown list. Values are:
  • Exact Match: Prevents communication if one of the following parameters do not match:
    • Vendor ID
    • Device Type
    • Product Code
    • Revision
  • Compatible Module: Communication occurs if the following parameters match:
    • Vendor ID
    • Device Type
    • Product Code
  • Disable Keying: Communication occurs regardless of whether the keying parameters match or not.
Connection
Select the connection for the configured device:
  • Data
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal