Off to On or On to Off value is under range
The Input Off -> On or On -> Off Filter Time value is blank or under the acceptable range for the device. Enter a value from 0 through 65, in resolutions of 1, and then apply the changes.
Provide Feedback