Off to On or On to Off value is over range

The Input Off -> On or On -> Off Filter Time value is blank or over the acceptable range for the device. Enter a value from 0 through 65, in resolutions of 1, and then apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal