Metering view parameters
Parameter | Description |
|---|---|
Nominal line - line voltage | Specifies the nominal system (line-to-line) voltage. Valid values range from 0.0 through 1,000,000.0. The default is
480. |
Nominal frequency | Specifies the nominal system frequency. Valid values are 50.0 Hz and 60.0 Hz (default). |
Metering mode | Configures the power monitor with the external electrical system and
how it is wired to the power monitor voltage and current input
terminals. The available values are:
|
Realtime update rate | Specifies the averaging used and the update rate of metering results
to the data tables and setpoint calculations. The available values are:
|
Potential Transformers | Configures the potential transformer or voltage transformer (PT of
VT) ratios that connect the power monitor to the electrical
system. If no PTs or VTs are used (direct connection), enter the same values
for the primary and secondary. |
V1,V2,V3 primary | Specifies the primary voltage rating of the voltage transformer
connected to V1, V2, and V3 of the power monitor. Valid values range from 0.0 through 1,000,000.0. The default value is
480.0. |
V1,V2,V3 secondary | Specifies the secondary voltage rating of the voltage transformer
connected to V1, V2, and V3 of the power monitor. Valid values range from 0.0 through 690.0. The default value is
480.0. |
V neutral primary | Specifies the primary voltage rating of the voltage transformer
connected to Vn of the power monitor. Valid values range from 0.0 through 1,000,000.0. The default value is
480.0. |
V neutral secondary | Specifies the secondary voltage rating of the voltage transformer
connected to Vn of the power monitor. Valid values range from 0.0 through 690.0. The default value is
480.0. |
I1,I2,I3 primary | Defines the transformation ratio of the current transformers (CTs)
used to sense current in the measured power circuit together with
the I1,I2,I3 secondary value.Valid values range from 0.0 through 1,000,000.0. The default is
5.0. |
I1,I2,I3 secondary | The CT secondary value is only permitted to be 5. |
I4 primary | Defines the transformation ratio of the current transformer (CT) used
to sense current in the neutral measured power circuit together with
the I4 secondary value.Valid values range from 0.0 through 1,000,000.0. The default is
5.0. |
I4 secondary | The CT secondary value is only permitted to be 5. |
Source | Use this value to select the source of the demand end-of-interval
(EOI) signal. The available values are:
The semantics are:
|
Number of periods | Specifies the number of demand periods to average for demand
measurement. Valid values are:
|
Period | Specifies the desired period for demand calculations. Valid values are:
The semantics are:
|
Forced synchronization delay | When configured for an external demand source, this value defines how
long the unit waits for the expected control input (for example, EOI
pulse or network demand broadcast), before it starts a new demand
period. If this occurs an entry is made in the Event Log. Valid values range from:
Tip: Network demand synchronization is available on units connected
to an Ethernet network. |
Broadcast mode | Configures the Demand Ethernet broadcast mode. The available values are:
|
Broadcast port | Specifies the port to be used for demand broadcast messages. Valid values range from 300 (default) through 400. |
Provide Feedback