Inputs view parameters
Parameter | Description |
|---|---|
Status Input Scale Factor | Displays the factor by which status inputs 1 thru 4 are to be
incremented for each off-to-on transition of the respective input.
Enter a desired value to change a scale factor. Select
Apply to set in the power monitor.Valid values range from 1 (default) through 1,000,000. If offline, the change will take effect when next online. |
Logic State Input | Displays the configuration of the logic state inputs for the KYZ
solid-state output and the relay outputs R1, R2 and R3. The
following values define the logic state input configuration for each
output. IMPORTANT: When a Data connection is active, the host Logix
controller owns the outputs and the user program determines their
state. The KYZLogicState, R1LogicState, R2LogicState and
R3LogicState tags in the <PowerMonitorName>.:I:0 tag display
output logic state based on the configuration. The power monitor
controls its outputs when there is no active Data connection, or
when an active Data connection faults and the fault response mode
(see below) is set to "Local Control". |
Mode | Determines the function that operates the respective output. The available values are:
|
Pulse Scale Factor | Determines the quantity of energy units that cause each transition of
the respective output when the selected Mode
is an energy unit (not equal to 0 = Setpoint Control). Valid values range from 1 through 100,000. The default is 1000. This
parameter is disabled when Mode is set to
Setpoint Control . |
Pulse Duration (ms) | Determines for the respective output if it toggles between off and
on, or how long in milliseconds it remains on following each
transition when the selected Mode is an
energy unit (not equal to 0 = Setpoint Control).Valid values are 0 ms (toggled operation) or from 50 through 1000 ms
(pulsed operation). The default is 250 ms. |
Provide Feedback