Conversion view parameters
The
Conversion
view includes these parameters:
TIP:
These parameters are not available in Run mode.
Parameter | Description |
|---|---|
Gray-to-Binary Convert | Select to convert the code type from Gray to Binary. |
Standardization | Select to apply standardization. |
Trailing Bits | Specify the trailing bits value if you are applying standardization. Valid values are in the range of 0...16. Trailing Bits is not available if Standardization is not applied and in Run mode. |
Sensor Resolution | Use this conversion formula for the sensor resolution:
For example, for a 40000 count sensor, the formula is: 40000 - 65536 = -25536. Valid values are in the range of 1...65535. |
Sensor Cycles | Use this conversion formula for sensor cycles:
For example, for a 50000 count sensor, the formula is: 50000 - 65536 = -15536. Valid values are in the range of 1...65535. |
Provide Feedback