Actual Gate Interval is out of range
The value is out of the range for the Actual Gate Interval. Enter a Gate Multiplier value and a Time Base value so that the product of these values is not higher than 3000 ms or lower than 10 ms.
Provide Feedback