Confirm the changes for Chassis Size in Device

Use this confirmation dialog box to verify that you wish to change the value displayed in the
Chassis Size in Device
field to match the values of the chassis size from the
Overview
view.
To confirm the changes for Chassis Size in Device
  • In the confirmation dialog box, select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal