Chassis Size view parameters

The
Chassis Size
view includes these parameters:
Parameter
Description
Chassis Size on Overview view
Displays the chassis size entered in the
Overview
view.
Chassis Size in Device
Displays the chassis size that is stored in the device.
Set Chassis Size in Device
Select to cause the value of
Chassis Size in Device
to match the value of the chassis size entered in the
Overview
view.
Set Chassis Size in Device
is unavailable when the chassis size entered in the
Overview
view matches the value displayed in
Chassis Size in Device
.
Refresh
Select to refresh the controls in the
Chassis Size
view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal