Module Properties dialog box - Safety General tab
Use the
Safety General
tab to create or view module properties for the safety modules. On this tab:- View the type and vendor of the module being created
- View the module parent
- Enter the name of the module
- Select the Slot
- Enter a description for the module
- View and change the Safety Network Number
- View or change the Module definition
Provide Feedback