Configure test output properties
Configure test output properties for the input module.
To configure test output properties for the input module:
- In theController Organizer, expand theI/O Configurationfolder, and double-click the module.
- SelectPoints.
- InPoint Mode, select the output mode of the test output.
- If available, selectDiagnosticto view diagnostic information about the point.
- SelectOK.
Provide Feedback