Enable HART invalid (input devices)

Enable HART is selected. To enable HART, these parameters must be set to the corresponding values:
  • Input Type = Current (mA)
  • Input Range = 4 mA to 20 mA
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal