System Power Alarms view parameters
The settings in the
Alarms
view enable or disable the 24V system power alarms and set the low and high voltage limits to trigger the system power alarms. The Alarms
view includes these parameters:Parameter | Description |
|---|---|
Enable System Power Alarms | Determines whether to enable or disable the high and low system power alarms. When the alarms are disabled, the High and Low System Power Alarm Limits are unavailable. |
High System Power Alarm Limit | Sets the trigger for the high system power alarm. When the voltage goes above this value, the high system power alarm transitions from off to on. |
Low System Power Alarm Limit | Sets the trigger for the low system power alarm. When the voltage goes below this value, the low system power alarm transitions from off to on. |
Provide Feedback