Configure system power alarm properties

Configure the alarm properties to trigger the system power alarms when system power exceeds high or low voltage limits.
TIP:
The
Alarms
view is only available when connection to the adapter is set to
Status
in
Device definition
.
To configure system power alarm properties
  1. On the tab for the device, select
    Alarms
    .
  2. In the
    Alarms
    view, select
    Enable System Power Alarms
    to enable the system power alarms.
  3. Enter values for these two parameters:
    • High System Power Alarm Limit
      Enter the maximum voltage allowed before the high system power alarm transitions from off to on.
    • Low System Power Alarm Limit
      Enter the minimum voltage allowed before the low system power alarm transitions from off to on.
  4. Select
    OK
    to save the change.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal