Refresh Diagnostics

Use
Refresh Diagnostics
after a communications error occurs and the resulting error message is acknowledged. Use
Refresh Diagnostics
to manually update the information currently displayed in the diagnostics dialog box and restart the timer that automatically updates the information displayed every five seconds.
To refresh diagnostics
  • In the diagnostics dialog box, select
    Refresh Diagnostics
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal