Configure device window parameters
Use the
Windows
view to view and configure device window parameters for the 5069-HSC2XOB4 high-speed counter device.
TIP:
Parameters not editable in the
Windows
view can be configured using device output tag members.To configure device window parameters
- On the tab for the device, selectWindows.
- In theWindowsview, fill in the parameters and selectOK.
Provide Feedback