Configure output parameters

Use the
Outputs
view to configure output parameters for the 5069-HSC2XOB4 high-speed counter device.
To configure output parameters
  1. On the tab for the device, select
    Outputs
    .
  2. In the
    Outputs
    view, fill in the parameters and select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal