Counter0x - Input view
Use the
Input
view to configure the inputs for the 5069-HSC2XOB4 high-speed counter device at the individual counter level.Input parameters vary depending on the operating mode. The operating modes are:
- Count/External Direction mode
- The B input controls the direction of the counter. If the B input is low (0), the counter increments on the rising edges of input A. If the input B is high (1), the counter decrements on the rising edges of input A.
- Count/Internal Direction mode
- The status of InvertDirectionInput, as controlled by the user program, determines the direction of the counter. The counter increments on the rising edge of the device’s A input when InvertDirectionInput is reset to 0. The counter decrements on the rising edge of the A input when InvertDirectionInput is set to 1.
- Up and Down Pulses mode
- The counter channel increments on the rising edge of pulses that are applied to input A and decrements on the rising edge of pulses that are applied to input B.
- X1 Quadrature Encoder mode
- A quadrature encoder is attached to inputs A and B, the phase relation of inputs A and B determine the count direction. If input A leads input B, the counter increments. If input B leads input A, the counter decrements.
- X2 Quadrature Encoder mode
- Operates much like X1 Quadrature Encoder mode except that the resolution is doubled.
- X4 Quadrature Encoder mode
- Operates much like X1 Quadrature Encoder mode except that the resolution is quadrupled.
Provide Feedback