Events view parameters

The
Events
view includes these parameters:
Parameter
Description
Member Name
Value
Enable Event
Determines whether the corresponding event trigger is active. Events are triggered once conditions match the definition.
EO.Event0x.En
0 = Event trigger definition is not active
1 = Event trigger definition is active
Latch Event
Determines what happens to the current event when a new event is received. When this parameter is selected, events are latched until acknowledged. A new event is lost if the previous event has not been acknowledged. When this parameter is not selected, new events overwrite old events.
EO.Event0x.LatchEn
0 = Event is not latched. New events overwrite old events.
1 = Event is latched. New events are lost if the latched event was not acknowledged.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal