User-defined data for events

The user-defined data selection made in
Device definition
modifies the configuration data type members for
AB:5000_HSC_Event_Struct:EI:0
and
AB:5000_HSC_Event4:EI:0
. This table lists and describes the combinations used to name
AB:5000_HSC_Event_Struct_xyz:EI:0
and
AB:5000_HSC_Event4_x0y0z0x1y1z1x2y2z2x3y3z3:EI:0
where:
  • x
    is the mask value of the enumerated value selected UserDefinedData00.
  • y
    is the mask value of the enumerated value selected UserDefinedData01.
  • z
    is the mask value of the enumerated value selected UserDefinedData02.
  • x0y0z0
    is the mask value of the structure in Event00.
  • x1y1z1
    is the mask value of the structure in Event01.
  • x2y2z2
    is the mask value of the structure in Event02.
  • x3y3z3
    is the mask value of the structure in Event03
    User-defined Data Selection
    Member Name
    Type
    C.AdditionalEventxDatay
    Mask Value
    No Additional Data
    UserDefinedx (x = 0, 1 or 2)
    Value is hidden in the EI structure
    DINT
    0
    A
    Stored Count
    StoredCount
    DINT
    1
    B
    Scaled Count
    ScaledCount
    REAL
    2
    C
    Scaled Stored Count
    ScaledStoredCount
    REAL
    3
    D
    Frequency
    Frequency
    REAL
    4
    E
    Average Frequency
    AverageFrequency
    REAL
    5
    F
    Stored Frequency
    StoredFrequency
    REAL
    6
    G
    Scaled Frequency
    ScaledFrequency
    REAL
    7
    H
    Scaled Average Frequency
    ScaledAverageFrequency
    REAL
    8
    I
    Scaled Stored Frequency
    ScaledStoredFrequency
    REAL
    9
    J
    Pulse Width
    PulseWidth
    REAL
    10
    K
    Average Pulse Width
    AveragePulseWidth
    REAL
    11
    L
    Stored Pulse Width
    StoredPulseWidth
    REAL
    12
    M
    Acceleration
    Acceleration
    REAL
    13
    N
    Average Acceleration
    Accel
    REAL
    14
    O
    Count
    Count
    DINT
    15
    P
    Revolution Count
    RevolutionCount
    INT (with INT pad)
    16
    Q
    Stored Revolution Count
    StoredRevolutionCount
    INT (with INT pad)
    17
    R
    Stored Acceleration
    StoredAccel
    REAL
    18
    S
    Scaled Acceleration
    ScaledAccel
    REAL
    19
    T
    Scaled Stored Acceleration
    ScaledStoredAccel
    REAL
    20
    U
    Scaled Acceleration Average
    ScaledAccelAvg
    REAL
    21
    V
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal