Device definition - Windows view

In
Device definition
, use the
Windows
view to define the mode for each window. The windows can trigger output behavior so that the output responds to input conditions at high speed.
To configure window definition parameters, make sure that
Connection
is set to
Data with Events
or
Data
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal