Device definition - Counters view

In
Device definition
, use the
Counters
view to define the operating mode of the counter and the Z terminal function associated with the counter. The mode of the counter determines how the A and B inputs cause a counter channel to increment or decrement. The device has two counters.
To configure counter definition parameters, make sure that
Connection
is set to
Data with Events
or
Data
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal