Counters view parameters

The
Counters
view includes these parameters:
Parameter
Description
Member Name
Value
Rollover
Shows the rollover value.
When the counter counts up to this value, it is set to the
Rollunder
value when the next pulse is received.
O.Counter0x.RolloverValue
-2147483648 to 2147483647 AND greater than the Rollunder value
Rollunder
Shows the rollunder value.
When the counter counts down to this value, it is set to the
Rollover
value when the next pulse is received.
O.Counter0x.RollunderValue
-2147483648 to 2147483647
Load Count Value
Shows the load count value.
O.Counter0x.LoadCountValue
O.Counter0x.Rollunder ≤ O.Counter0x.LoadCountValue < O.Counter0x.Rollover
Load Revolution Value
Shows the load revolution value.
O.Counter0x.LoadRevolutionValue
-32768 to 32767
Scalar
Specifies the scaling value for the counter.
  • Scale count, frequency, and acceleration values to Engineering Units in REAL by multiplying their integer values in pulses by the Scaling value.
  • For example: For motion applications, scale count, frequency, and acceleration to position, velocity, and acceleration/deceleration.
C.Counter0x.Scaling
32-bit floating point value
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal