Invalid test source

Only test outputs configured as
Safety Pulse Test
can be used as test sources. A test output can be associated with zero, one, or two safety input channels.
Check the configuration and make the required modification.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal