Invalid Enable No Load Detection combination

The
Enable No Load Detection
values cause an invalid combination for the pair of points.
If
Point Operation Type
is
Dual
, use the same
Enable No Load Detection
checkbox setting for the two output points.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal