Overview view parameters (5034-UB8, 5034-UB8F)
The
Overview
view includes these parameters:
Parameter | Description |
|---|---|
Series | Displays the series of the device. |
Revision | Displays the revision of the device. |
Electronic Keying | Displays the electronic keying that is used for the device. |
Connection | Displays the connection type and the communication format. |
MAOC Compatible Data | Specifies whether the data is compatible with Motion Arm Output
Cam (MAOC) instruction. If the data is not compatible with MAOC, you cannot use this
module with MAOC instruction. Some point assignment options are not available when Yes is
selected. |
Timestamp (For 5034-UB8F only) | Specifies how the timestamp information is saved and reported for
the digital input events.
|
Points Assignments | Displays the operating mode that is assigned for each point. |
Device Definition | Opens Device definition dialog to change the revision, electronic
keying, point mode, and other device-specific values. |
Provide Feedback