Input Eventxx view parameters (5034-UB8F)
The
Input Eventxx
view includes these parameters.Parameter | Description | Member Name | Value |
|---|---|---|---|
Enable Event | Displays whether the corresponding event trigger is active. Events are triggered
when conditions match the event definition. | EO.Eventxx.En |
|
Latch Event | Displays whether an event is latched until it is acknowledged. | EO.Eventxx.LatchEvent |
|
Enable Independent Point Triggers | Displays whether each condition indicated in the Event trigger definition can
initiate an event independently. | EO.Eventxx. IndependentConditionTriggerEn |
|
Trigger Event | Triggers an event each time an input state change results in one of the following
conditions:
|
| Values (EventRisingEn, EventFallingEn) represent:
|
Event Trigger Pattern – Participate in Event Trigger | Displays whether the specified point participates in the Event trigger definition
for the event. |
|
|
Event Trigger Pattern – State Transition | Displays the state of the input to match after the transition. |
| For PtxxDataValue:
For CounterxxValue:
|
Provide Feedback