Input Events view parameters (5034-UB8F)
The
Input Events
view include these parameters:Parameter | Description | Member Name | Value |
|---|---|---|---|
Event | The event number to which this configuration applies. | — | — |
Enable Event | Displays whether the corresponding event trigger is active. Events are triggered
when conditions match the event definition. | EO.Eventxx.En |
|
Latch Event | Displays whether an event is latched until it is acknowledged. | EO.Eventxx.LatchEvent |
|
Provide Feedback