Device Definition view

Use
Device Definition
to:
  • Define the device revision.
  • Select the electronic keying.
  • Configure device-specific settings.
TIP: The parameters are based on the device being configured. The parameters that do not apply to the device are hidden.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal