Ptxx Diagnostics view parameters (5034-OB16, 5034-OB8, 5034-OB4)

The
Ptxx Diagnostics
view includes these parameters:
Parameter
Description
Fault Exists
Displays whether a fault is present.
Data Uncertain
Displays the module is operating outside the designed operating range, or data is under manual or override control.
Field Power
Displays whether field power is present on the point.
Field Power On Timestamp
Displays the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Field Power Off Timestamp
Displays the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Short Circuit Fault
Displays whether a short circuit fault is present on the point.
Short Circuit Fault Timestamp
Displays the timestamp of the last short circuit fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
No Load Fault
Displays whether a No Load fault is present on the point.
No Load Fault Timestamp
Displays the timestamp of the last No Load fault in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time was recorded.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal