Points view parameters (5034-OW4I)
The
Points
view includes these parameters:
Parameter | Description |
|---|---|
Point | Displays the point number to which this configuration
applies. |
Output State During Program Mode | Determines the behavior of each output when the controller
transitions to Program Mode or Inhibit mode. While in
Program Mode or Inhibit mode, outputs from the controller
are ignored and the output behaves as follows:
|
Output State During Communication Fault Mode | Determines what happens to the output of each point after a
communication fault occurs and the module enters
Communication Fault Mode.
|
Communication Fault Mode Output State Duration | Determines the length of time the Communication Fault Mode is
held before the Final Fault State. |
Communication Fault Mode Output State Final State | Determines whether the module transitions to On or Off after
the Communication Fault Mode Output State Duration elapses.
The default final state is Off. If you choose Forever for Duration, you cannot choose a final
state. The module retains its current Communication Fault
Mode state. |
Mode When Communication Fails in Program Mode | Determines the output action if communication fails in
Program Mode.
|
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Provide Feedback