Channels view parameters (5034-OF4IH)
The
Channels
view include these parameters:Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration applies. |
Disable | Determines whether the channel is disabled. Disable channels to prevent erroneous
fault reporting, such as No Load or Open Wire faults, and to prevent the fault
indication from the channel status indicator. |
Output Type | Sets the output type for the channel. Available options are:
|
Output Range | Sets the output range for the output type. Ranges vary based on the selected
Output Type. |
Enable HART | Enables communication to HART devices. |
Output State During Program Mode | Determines the channel action when the controller transitions to Program Mode or
Inhibit mode.
|
Output State During Communication Fault Mode | Determines the channel action when a communication fault occurs.
|
Enable No Load Detection | Determines whether No Load Detection is enabled for the channel.
IMPORTANT:
This option is available only if the Input Type is Current. |
High Signal | Sets one of the four constants in the scaling equation. High Signal is in terms
of the input signal units and corresponds to High Engineering when scaled. |
Low Signal | Sets one of the four constants in the scaling equation. Low Signal is in terms of
the input signal units and corresponds to Low Engineering when scaled. |
Engineering Units | Sets the unit of measurement for High Engineering and Low Engineering. |
High Engineering | Sets one of the four constants in the scaling equation. High Engineering
corresponds to High Signal and helps determine the engineering units that the
signal values scale into. |
Low Engineering | Sets one of the four constants in the scaling equation. Low Engineering
corresponds to Low Signal and helps determine the engineering units that the
signal values scale into. |
Recalculate Units | Recalculates new values to the following configuration parameters in Engineering
Units based on the new Scaling constants.
TIP:
This option is enabled when any of the four
Scaling constants is changed.
|
Provide Feedback