Calibration Wizard parameters
The
Calibration Wizard
includes these parameters:
Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration
applies. |
Calibrate | Identifies the channels for calibration. Select the check box that corresponds to the channel number you
want to calibrate. |
Calibration Range | Displays the value currently configured for the channel. Values
display according to the Input Type selected. |
Calibration Gain | Displays the calibration gain values as reported by the
module. |
Calibration Offset | Displays the offset in signal units as reported by the
device. |
Calibration Status | Displays the status of the calibration per channel as the
calibration occurs. |
Calibrate Channels in Groups | Select this check box if you want to calibrate multiple channels
as a group. |
Calibrate Channels One at a Time | Select this check box to calibrate one channel at a time. |
Low Reference | Displays the value of the low reference signal for the
channel. |
High Reference | Displays the value of the high reference signal for the
channel. |
Recorded Reference | Indicates the measured output values. |
Low Recorded | Displays the recorded low reference value in signal units. |
High Recorded | Displays the recorded high reference value in signal units . |
Status | Displays the value read during calibration for the enabled
channels.
If Status shows Error, measure and enter the recorded reference
values again for the channels in error, and then select
Retry. |
Provide Feedback