Output Logic view parameters
The
Output Logic
view includes these parameters:Parameter | Description |
|---|---|
Peer Module | The type of the peer input device. The input device must be in the same chassis as the 1756-OB16IEF output device. Choose the device from the menu.
Tip : To include a peer device in the Peer Module list, the device must be added to I/O tree before attempting to configure the 1756-OB16IEF Output Logic. |
Peer Slot | Choose the peer slot from the list. |
Logic Configuration Grid | The operators and operands that define the expression for each output point. |
Provide Feedback