Average Frequency Over value is over range

The Average Frequency Over value is greater than the maximum of 1000. Enter a value from 0 through 1000 and apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal