User-defined value is not within clamp limits
The user-defined value for limit values.
Output State in Program Mode
is not within the range of the high clamp and low clampChange the low clamp or high clamp value or enter a user-defined value that is within the acceptable range, and then save the changes.
Provide Feedback